This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140: Connect -5V/+5V preamp output to 3.3V ADC

Part Number: TLV320ADC6140


I need to connect a measurement microphone + preamplifier to a TLV320ADC6140 input.

The preamplifier is powered symmetrically with +5.5V and -5.5V so the signal is single ended and voltage vary in the range -5.5V/+5.5V which is not ADC input range (0-3.3V)

Does somebody can recommend a design for that situation ?

Thanks a lot !