Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2906C: PCM2906C internal power supply pin

Part Number: PCM2906C

Hello, I have an issue with a product design using PCM2906C.

Are any of the VCCCI, VDDI, or VCCXI pins to which the internal power supply is connected acceptable up to 1.8 mA output?

  • Hi Rio,

    The current rating for the internal analog power supplies is not explicitly stated in the datasheet, but considering that the typical voltage is for those pins is 3.3V and typical power dissipation is 280mW (Pd is calculated from all power supplies) I would assume that 1.8mA is acceptable.