This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3254EVM-K: TLV320AIC3254EVM-K: PurePath I2S problem

Part Number: TLV320AIC3254EVM-K


Hi

I am trying to program a simple application with an I2S microphone and an I2S amplifier at the output, using purepath 5.95

after building, and executing "Download & run", the program detects the board and that it has loaded the firmware well.

But the program does nothing, I have no audio output in the amplifier; and when I modify values in the GEQ_5_1 block, it returns an error

Do you have an example project on purepath to check the I2S audio output, or what can I do to check if the program is running ok?