Other Parts Discussed in Thread: LM675, OPA548, TPA3118D2
Hi Expert,
My customer is considering the signal amplifier with D-amp (not audio)
Input 0 to 3.3V (Trapezoidal wave, Tr=Tf=10us)
Output 0 to 24V
Load condition
RC x 1000circuits
R=100ohm, C=75pF
Peak current is estimated 0.5mA/ 1 RC circuit
Total current max : 500mA (=0.5mA x 1000 circuit)
Could you please let me know the recommended device, If D-amp can drive this configration? TPA3123D2?
Or, should they use the Power amp? like LM675, OPA548.
Also, do you have TPA3123D2 spice model?
Thanks
Muk