Part Number: RC4580-Q1
Other Parts Discussed in Thread: TS5A22364-Q1, RC4580, TLV9002, TINA-TI
Hi Team,

Please review the above schematic attached, I need to confirm if it is good for stereo audio out from the audio jack of laptop.
What should be the connection on a non-inverting pin of OPAMP in case of inverting input?
1. I have fed it the same GND_LP as the audio jack.
2. Two channel inputs (LP_AUDIO_L/LP_AUDIO_R) are the outputs of audio mux TS5A22364-Q1.
3. Before this stage, two audio jacks are giving input to the audio mux.
Second, do this OPAMP need a Low pass filter stage on inverting input? also, review the inverting input RC circuit.