Other Parts Discussed in Thread: CC8520, PCM1773, MSP430F5438
Hi All,
Question 1
I build a prototype board which using CC8520+PCM1773 for DAC, I found that when CC8520 cannot receive the RF signal from TX side, the audio signal will stop with Pop noise, but Pop noise issue is not appear in CC85xxDK kit, any advise? as I know that CC8520 provide a mute function when the RF link broken, I would like to clarify that the mute function is provided by CC8520 stop I2S data out or CC8520 through I2C to send mute command to DAC?
Question 2
How to fix the RF channel, because CC8520 is using frequency hopping, I want to measure the output power on my prototype board.
Question 3
Any reference source code of MSP430 when CC8520 work as slave, for example CC8520 provide AD0 & AD1, I want to switch between these two input without "Pure path wireless configurator"
Question 4
I'm prepare goto production now, each TX & RX board will be program to different product ID, but it another product which using CC8520 too, maybe Product ID are same, what would be happen?
Question 5
How to generate different Product ID under "Pure path wireless configurator"
Question 6
When go for production and perform testing, may I pre pair TX & RX board when download the FW from "Pure path wireless configurator" because I don't want to pair one by one in production line
BR
Edwin