Hi,
I have asked this question before on another thread started by another person - but thought i would initiate a thread for this question.
For the PCM1792A - the datasheet figure 36 indicates that the I/V converter (NE5534) has the Positive input tied directly to ground.
Q1. Would the circuit perfromance benefit if the Positive terminal of this Op Amp was connected to ground through a resistor whose resistance is equivalent to the output impedance of the PCM1792A. ?
If we assumed that the average output is 25% of the peak output - thus output current is 1.95mA on average - which could be considered to be 500ohms approx output impedance - would this be an reasonable value to use ?.
Or is the output circuit of the PCM1792A an equivalent Nortons current generator with associated static (?) impedance ?.
If so - what is the output impedance ?. Thanks.
Regards,
Richard.