Other Parts Discussed in Thread: PCM9211
Dear, TI Support Team
Inquiries have been received from customers regarding the specifications of TAS5806MD.
[Inquiry 1]
If you look at the TAS5806MD specification sheet, there is a DC OFFSET DETECT function as shown below, but the exact SPEC is not shown.

Please check what happens to Normal, Max DC voltage during normal operation and DC Detect voltage for protection operation.
It is a necessary part to set the standard when measuring SPEC, so please check it.
[Inquiry 2]
The product under development is 25W+25W (8ohm 1KHz THD 1%) basic specification, and PVDD 24V / 4~16ohm impedance is used.
If you look at the specifications below, it is MIN 4.8ohm when PVDD 24V / BLT method is used.

Please check if there are any problems or absolute conditions when using under 4ohm conditions.
[Inquiry 3]
As shown in the block diagram below, if the OPTICAL (SPDIF) sampling frequency is 192KHz, it is not supported by the TAS5806MD, so another alternative AMP IC is required.

Please check if there is an alternative with the same performance as the TAS5806MD.
And please check whether sampling frequency conversion is possible in PCM9211. (Is down sampling possible?)
Thanks.
Regards,
MJ