This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3110D2: 5W Mono PA selection

Part Number: TPA3110D2

Hi Team, 

My customer need a PA, they used to use 3W but volume too small so they want to upgrade. Below are the key parameters,

 

Output power

~5W, mono

Power Supply

5V or 12V

Load

4Ωor 8Ω

Temp

-40~85

Others

No diagnostic needed

ON/OFF control

 

Customer prefer classD, I promoted TPA3111D but size is too big and lots of reductant pin. Do you have any other recommendation?