Other Parts Discussed in Thread: LMP7731, OPA1632, LM4562,
We currently utilize a Cirrus Logic ADC (stereo, I2S master) in our main product but were researching alternatives; our plan was originally to switch to ESS but we've changed our mind. So, as this was the only chip in our design that wasn't TI, we figured we would explore the TI audio ADC lineup and have a 100% TI design.
Our device input is single-ended (basically consumer line level audio) to differential input buffer based on the OPA1632 (almost exactly like OPA1632 datasheet, page 18) except with two independently buffered Vref via LMP7731 (one per channel). Our input buffer power supply is +/- 10V.
We are hoping to migrate to the LM4562 (for availability reasons) on our input buffer but we're not sure if buffering is even required on this ADC to realize the specified noise / distortion performance. In addition to this, we are wondering if you can give us a schematic (as a starting point) to take advantage of summing the 4 inputs into 2 (stereo) however on page 35 of the TLV320ADC5140 datasheet (8.3.6.6 Programmable Channel Summer and Digital Mixer) we can't determine how to interface our input buffer to the analog input pins. We should be able to figure out I2C from there.
Our goal is simply to achieve the specified noise and distortion performance and maximize stereo separation (at any cost). Any suggestions from the TI engineering team would be very appreciated.
Our current dbFS is: 18dBu, ~15.78dBV, ~17.4Vpp, ~6.15Vrms.
Thank you!