Hi there,
I've made a testing board of TAS5558 for our internal use. The schematic is attached.
I've burned the USB-AudioEVM0354_48KHZ.bin into the EEPROM. The Green LED (LED 1) lights up when I connect the board to PC and the PC shows that audio output device is now USB-AudioEVM. All the jumping wires are set to get all signals from the TAS1020B which means it's circuit almost identical to the TAS5548EVM. When I press connect button on PPC1 (v1.16). The VALID LED lights up and the PWM channels start to give a 50% duty PWM signals with pulse width of 2.6us (384kHz). When I play music from PC, however, the PWM 1 and 2 still keep giving me a 50% PWM signals that mean no sound I can get from the headphone jack.
Then I power cycled the board and let all the registers in TAS5558 start from default values. And I set the following registers manually: 0x03 -> 0x0A, 0x12 -> 0x00, 0xD9 -> 00-00-00-48. But the VALID LED still not goes up. Once I change the value of the register 0x04 from 0x03 to 0x53. The VALID LED lights up but the PWM1 and PWM2 still give me a 50% duty output. No sound at all.
I've studied the support forum about the TAS55x8 issues. Someone suggest that if the OSCRES resistor is not exactly 18k ohm, the pwm output will keep in mute state. I've measured the OSCRES resistor which has a resistance of 17.998k ohm using a digital multi-meter.
I've monitored all the input signals of the TAS5558. 48kHz clock is meaured at pin 22, 3.072MHz clock is measured at pin 23. 12.288MHz clock is measured at pin 11. A 16-bit I2S dat signal is present at the pin 24. All VR pins gives about 1.8v readings. And all power input pin seems in normal condition. The XC6214 voltage regulator can deliver at least 500mA current. Two set of register dumps I've used are listed as following:
1. Registers dump when after I press connect button in PPC1:
X00 6C
X01 04
X02 00
X03 A0
X04 53
X05 E0
X06 E0
X07 E0
X08 E0
X09 E0
X0A E0
X0B E0
X0C E0
X0D 00
X0E 55
X0F 00
X10 0A
X11 91
X12 00
X13 80
X14 44
X15 02
X16 77
X17 77
X18 77
X19 77
X1A 55
X1B 80
X1C 00
X1D C0
X1E 40
X1F A0
X20 20
X21 E0
X22 60
X23 00
X24 0F
X25 80
X26 FF
X27 00
X28 10
X29 55
X2A 55
X2B 55
X2C 55
X2D 00
X2E 00
X2F 00
X30 01
X31 23
X32 45
X33 67
X34 01
X35 23
X36 45
X37 67
X38 80
X39 00
X3A C0
X3B 40
X3C A0
X3D 20
X3E E0
X3F 60
X40 00 00 FF 00
X41 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X42 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X43 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X44 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X45 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X46 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00
X47 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00
X48 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00
X49 00 00 00 00
X4A 00 00 00 00
X4B 00 00 00 00
X4C 00 00 00 00
X4D 00 80 00 00
X4E 00 00 00 00
X4F 00 00 00 00
X50 00 80 00 00
X51 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X52 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X53 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X54 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X55 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X56 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X57 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X58 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X59 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X60 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X61 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X62 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X63 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X64 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X65 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X66 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X67 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X68 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X69 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X70 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X71 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X72 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X73 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X74 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X75 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X76 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X77 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X78 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X79 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X80 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X81 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X82 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X83 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X84 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X85 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X86 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X87 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X88 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X89 00 80 00 00 00 00 00 00
X8A 00 80 00 00 00 00 00 00
X8B 00 80 00 00 00 00 00 00
X8C 00 80 00 00 00 00 00 00
X8D 00 80 00 00 00 00 00 00
X8E 00 80 00 00 00 00 00 00
X8F 00 80 00 00 00 00 00 00
X90 00 80 00 00 00 00 00 00
X91 0F C0 00 00
X92 00 00 00 00
X93 00 00 00 00
X94 00 00 00 00
X95 00 FE 50 45 0F 81 AA 27 00 00 D5 13 00 00 00 00 0F FF 2A ED
X96 00 00 00 00
X97 00 00 00 00
X98 00 00 44 32 00 7F BB CE
X99 0B 20 E2 B0 06 F9 DE 57
X9A 00 40 00 00 0F C0 00 00 0F 90 00 00
X9B FF 82 30 98 01 95 B2 C4
X9C 00 00 44 32 00 7F BB CE 00 00 AA 39 00 7F 55 C7
X9D 00 00 44 32 00 7F BB CE
X9E 0B 20 E2 B0 06 F9 DE 57
X9F 00 40 00 00 0F C0 00 00 0F 90 00 00
XA0 FF 82 30 98 01 95 B2 C4
XA1 00 00 44 32 00 7F BB CE 00 00 AA 39 00 7F 55 C7
XA2 00 80 00 00 00 00 00 00
XA3 00 80 00 00 00 00 00 00
XA4 00 80 00 00 00 00 00 00
XA5 00 80 00 00 00 00 00 00
XA6 00 80 00 00 00 00 00 00
XA7 00 80 00 00 00 00 00 00
XA8 00 80 00 00 00 00 00 00
XA9 00 80 00 00 00 00 00 00
XAA 00 80 00 00 00 00 00 00
XAB 10 80 00 00 00 00 00 00
XAC 20 80 00 00 00 00 00 00
XAD 30 80 00 00 00 00 00 00
XAE 40 80 00 00 00 00 00 00
XAF 50 80 00 00 00 00 00 00
XB0 60 80 00 00 00 00 00 00 00 00 00 00
XB1 70 80 00 00 00 00 00 00 00 00 00 00
XB2 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
XB3 00 00 00 00
XB4 00 00 00 00
XB5 00 00 00 00
XB6 00 00 00 00
XB7 00 00 00 00
XB8 00 00 00 00
XB9 00 00 00 00
XBA 00 00 00 00
XBB 00 00 00 00
XBC 00 00 00 00
XBD 00 00 00 00
XBE 00 00 00 00
XBF 00 00 00 00
XC0 00 00 00 00
XC1 00 00 00 00
XC2 00 00 00 80
XC3 00 50 11 10
XC4 00 01 00 55
XC5 00 00 00 00
XC6 00 00 00 00
XC7 00 00 00 00
XC8 00 00 00 00
XC9 00 00 00 00
XCA 00 00 00 00
XCB 00 00 00 00
XCC 00 00 00 00
XCD 00 00 00 00
XCE 00 00 00 00
XCF 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
XD0 00 00 01 3F
XD1 00 00 00 48
XD2 00 00 00 48
XD3 00 00 00 48
XD4 00 00 00 48
XD5 00 00 00 48
XD6 00 00 00 48
XD7 00 00 00 48
XD8 00 00 00 48
XD9 00 00 00 70
XDA 03 03 03 03
XDB 12 12 12 12
XDC 03 03 03 03
XDD 12 12 12 12
XDE 00 00 00 00
XDF 00 00 00 02
XE0 00 00 00 00
XE1 00 00 00 00
XE2 FF FF 10 10
XE3 00 29 03 33
XE4 00 1C FE EF
XE5 00 1C FE EF
XE6 00 1C FE EF
XE7 0F E3 01 11
XE8 0F E3 01 11
XE9 00 80 00 00
XEA 00 80 00 00
XEB 00 00 00 00
XEC 00 00 00 00
XED 00 00 00 00
XEE 00 00 00 00
XEF 00 00 00 00
XF0 00 00 00 00
XF1 00 00 00 00
XF2 00 00 00 00
XF3 00 00 00 00
XF4 00 80 00 00
XF5 00 00 00 00
XF6 00 00 00 00
XF7 00 00 00 00
XF8 00 00 00 00
XF9 00 00 00 34
XFA 00 00 00 00
XFB 00 29 03 33
XFC 00 29 03 33
XFD 00 00 00 00
XFE 00 00 00 00
XFF 00 00 00 00
2. Registers dump after I power cycled the board, andonly made changes on 0x03, 0x04, 0x12 and 0xD9
X00 6C
X01 04
X02 00
X03 A0
X04 53
X05 E0
X06 E0
X07 E0
X08 E0
X09 E0
X0A E0
X0B E0
X0C E0
X0D 00
X0E 55
X0F 00
X10 0A
X11 91
X12 00
X13 80
X14 44
X15 02
X16 77
X17 77
X18 77
X19 77
X1A 55
X1B 80
X1C 00
X1D C0
X1E 40
X1F A0
X20 20
X21 E0
X22 60
X23 00
X24 0F
X25 80
X26 FF
X27 00
X28 10
X29 55
X2A 55
X2B 55
X2C 55
X2D 00
X2E 00
X2F 00
X30 01
X31 23
X32 45
X33 67
X34 01
X35 23
X36 45
X37 67
X38 80
X39 00
X3A C0
X3B 40
X3C A0
X3D 20
X3E E0
X3F 60
X40 00 00 FF 00
X41 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X42 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X43 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X44 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X45 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X46 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00 00 00 00 00
X47 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00 00 00 00 00
X48 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 80 00 00
X49 00 00 00 00
X4A 00 00 00 00
X4B 00 00 00 00
X4C 00 00 00 00
X4D 00 80 00 00
X4E 00 00 00 00
X4F 00 00 00 00
X50 00 80 00 00
X51 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X52 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X53 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X54 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X55 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X56 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X57 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X58 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X59 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X5F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X60 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X61 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X62 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X63 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X64 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X65 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X66 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X67 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X68 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X69 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X6F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X70 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X71 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X72 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X73 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X74 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X75 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X76 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X77 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X78 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X79 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7A 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7B 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7C 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7D 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7E 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X7F 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X80 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X81 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X82 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X83 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X84 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X85 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X86 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X87 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X88 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
X89 00 80 00 00 00 00 00 00
X8A 00 80 00 00 00 00 00 00
X8B 00 80 00 00 00 00 00 00
X8C 00 80 00 00 00 00 00 00
X8D 00 80 00 00 00 00 00 00
X8E 00 80 00 00 00 00 00 00
X8F 00 80 00 00 00 00 00 00
X90 00 80 00 00 00 00 00 00
X91 0F C0 00 00
X92 00 00 00 00
X93 00 00 00 00
X94 00 00 00 00
X95 00 FE 50 45 0F 81 AA 27 00 00 D5 13 00 00 00 00 0F FF 2A ED
X96 00 00 00 00
X97 00 00 00 00
X98 00 00 88 3F 00 7F 77 C0
X99 0B 20 E2 B2 06 F9 DE 58
X9A 00 40 00 00 0F C0 00 00 0F 90 00 00
X9B FF 82 30 98 01 95 B2 C0
X9C 00 00 88 3F 00 7F 77 C0 00 00 00 56 00 3F FF A8
X9D 00 00 88 3F 00 7F 77 C0
X9E 0B 20 E2 B2 06 F9 DE 58
X9F 00 40 00 00 0F C0 00 00 0F 90 00 00
XA0 FF 82 30 98 01 95 B2 C0
XA1 00 00 88 3F 00 7F 77 C0 00 00 00 56 00 3F FF A8
XA2 00 80 00 00 00 00 00 00
XA3 00 80 00 00 00 00 00 00
XA4 00 80 00 00 00 00 00 00
XA5 00 80 00 00 00 00 00 00
XA6 00 80 00 00 00 00 00 00
XA7 00 80 00 00 00 00 00 00
XA8 00 80 00 00 00 00 00 00
XA9 00 80 00 00 00 00 00 00
XAA 00 80 00 00 00 00 00 00
XAB 10 80 00 00 00 00 00 00
XAC 20 80 00 00 00 00 00 00
XAD 30 80 00 00 00 00 00 00
XAE 40 80 00 00 00 00 00 00
XAF 50 80 00 00 00 00 00 00
XB0 60 80 00 00 00 00 00 00 00 00 00 00
XB1 70 80 00 00 00 00 00 00 00 00 00 00
XB2 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
XB3 00 00 00 00
XB4 00 00 00 00
XB5 00 00 00 00
XB6 00 00 00 00
XB7 00 00 00 00
XB8 00 00 00 00
XB9 00 00 00 00
XBA 00 00 00 00
XBB 00 00 00 00
XBC 00 00 00 00
XBD 00 00 00 00
XBE 00 00 00 00
XBF 00 00 00 00
XC0 00 00 00 00
XC1 00 00 00 00
XC2 00 00 00 80
XC3 00 50 11 10
XC4 00 01 00 55
XC5 00 00 00 00
XC6 00 00 00 00
XC7 00 00 00 00
XC8 00 00 00 00
XC9 00 00 00 00
XCA 00 00 00 00
XCB 00 00 00 00
XCC 00 00 00 00
XCD 00 00 00 00
XCE 00 00 00 00
XCF 00 80 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
XD0 00 00 01 3F
XD1 00 00 00 48
XD2 00 00 00 48
XD3 00 00 00 48
XD4 00 00 00 48
XD5 00 00 00 48
XD6 00 00 00 48
XD7 00 00 00 48
XD8 00 00 00 48
XD9 00 00 00 48
XDA 03 03 03 03
XDB 12 12 12 12
XDC 03 03 03 03
XDD 12 12 12 12
XDE 00 00 00 00
XDF 00 00 00 02
XE0 00 00 00 00
XE1 00 00 00 00
XE2 FF FF 10 10
XE3 00 29 03 33
XE4 00 1C FE EF
XE5 00 1C FE EF
XE6 00 1C FE EF
XE7 0F E3 01 11
XE8 0F E3 01 11
XE9 00 80 00 00
XEA 00 80 00 00
XEB 00 00 00 00
XEC 00 00 00 00
XED 00 00 00 00
XEE 00 00 00 00
XEF 00 00 00 00
XF0 00 00 00 00
XF1 00 00 00 00
XF2 00 00 00 00
XF3 00 00 00 00
XF4 00 80 00 00
XF5 00 00 00 00
XF6 00 00 00 00
XF7 00 00 00 00
XF8 00 00 00 00
XF9 00 00 00 34
XFA 00 00 00 00
XFB 00 29 03 33
XFC 00 29 03 33
XFD 00 00 00 00
XFE 00 00 00 00
XFF 00 00 00 00