This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM2912: Design applications/solutions

Part Number: PCM2912

Hi Experts,

Seeking your help on this query from Cx:

I am looking for some information on whether the PCM2912 is a suitable IC for our application. We need a solution which allows us to connect an 3.5mm headset to the PC using the USB port (ie. like a USB to 3.5mm Audio adapter). Is the PCM2912 a popular chip for this type of application? Seems an NRND, is the PCM2912A work also?

Lastly, we're also looking for a simple solution to add a 4-port usb 3.0 hub functionality into our product and would appreciate any recommendations from your experts.

Regards,
Archie A.