Part Number: TAS5614
Hi,Team
The customer is currently using Tas5534+Tas5614, there are 2 problems as follows, (AMP power supply voltage: 25V, load 4 ohms)
1: When the input is -24db, there is 2.6% distortion measured at the speaker end, and the output is about 10W. (Distortion occurs when the input is slowly increased from -30db to around -24db, and if it is increased, such as -22db, the distortion is normal; if it is slowly decreased from -20db to -24db, the distortion looks OK), this is what is the problem? software configuration?


2: At the moment when the signal is turned on, there is a pulse, as shown in the figure below, is there a problem with the software configuration?