This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424e_q1 channel 2 can't output audio

Other Parts Discussed in Thread: TAS6424E-Q1, TAS6424E, TAS6424

About TAS6424e-q1 channel 2 , it can't output audio signal, why?   but channel 1, channel3/4 can output audio.

now I use TAS6424e, my usage is like this : channel 3 and channel 4 is  PBTL output, channel1/channel 2 is btl output;  schematic is refer to typical reference of TAS6424e,

the register set is like this (left colum is register address, right colum is value):

register, value:

0x00,   0x20

0x01,    0x23

0x02,     0x71

0x03,    0x54

0x04,    0x00

0x05,    0xD0

0x06,    0xD0

0x07,    0xD0

0x08,   0xD0

0x21,    0x00

0x28,    0x2A

and audio input is 16bit I2S data, sample rate is 48K hz , stereo sample, wav data file.  MCLK is 12.288MHZ ,  LR clock is fs=48KHZ, 

bclk is 64*fs, data bit speed is 32*fs, I use stm32f407 produce audio source.