Hi All
In my app, I have 2 stereo analog inputs connected to LINE 1 and 2 L/R.
In addition to those 2 analog inputs, I have a I2S input.
I want to mix all those 3 inputs and forward them to LINE OUT L/R.
Inside the codec, I can do this mix, but I'd like to be able to apply the 2 bands equalizer on the mixed signals, before going to the line outputs.
From my understanding, it seems the block before the effects is a multiplexor, not a mixer. So basically the input of the effects is the output of the ADC OR the digital input.
Is this correct ?
If I close the switch SW-D1 shown in block diagram page 18, continue using the I2S inputs, and keep the DAC ON, will the effects block receive the mix of ADC OUT + I2S IN ?
I'd like to avoid using an additional DAC for I2S input, just to be able to mix 3 analog inputs before going to the effects, that would result in DIGITAL -> ANALOG -> DIGITAL -> EFFECTS -> ANALOG, which makes no sense.
Thanks for clarifying
Jerome