Part Number: RC4558
Hello,
I have a question about the output amplitude characteristics of RC4558.
What is the maximum output amplitude at RL=12kohm, VCC=±12V, T=0~55℃?
I would like an output amplitude of ±10V.
Regards,
Keitaro Arai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: RC4558
Hello,
I have a question about the output amplitude characteristics of RC4558.
What is the maximum output amplitude at RL=12kohm, VCC=±12V, T=0~55℃?
I would like an output amplitude of ±10V.
Regards,
Keitaro Arai
Hello Keitaro,
The 10k specification will be helpful. It shows a typical 1V loss and a limit of 3V loss. This is at 1.2mA (12V/10k)
For the desired 10V output, current would be 0.83mA. (70% of 1.2mA)

So it will certainly be better than a 3V loss which is +/-9V at 12V supply. The worst than worst case analysis is not good enough for 10V.
Sample data for VOL is a 1.65V loss at 25C. 12V * 95% - 1.65V = 9.75V. Therefore getting 10V is not going to happen with 12V +/-5%.