This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211: [ESTEC] Inquire about PCM9211 AD features

Part Number: PCM9211

Hi, TI support team

I have received the following inquiries from our customers.

Please check the contents of the inquiry and BLOCK DIAGRAM before responding.

******************************************************************************************************************

We are trying to operate the new model using the A/D function of the PCM9211.

In case of A/D input, PCM9211 ( MPIO_C ) is input for MCLK/BCK/LRCK and Data is output.

- Sampling will use 44.1kHz

At this time, Main Output should output A/D signal normally.

Is it possible to implement that function?

******************************************************************************************************************

Thanks.

Regards,

MJ