Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV135: i don`t understand Tina ti simulation result why gain error occur with 10%

Part Number: DRV135

Hellow 

i`m analyze drv135 Using TINA ti

but I don`t understadnd Simulation result 

in this condition V+ :15V, V-:-15V Vin;3V, Vo+ is 3.3V and Vo- is -3.28V 

in datasheet, Gain error is noticed 0.1% at Diffrential 

so, i have a question that  DRV135`s Gain error  is 0.1% actually

please help me

thank you