This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS6424-Q1: Frequency of I2S

Part Number: TAS6424-Q1


I am developing Audio System using TAS6424QDKQRQ1, and have a question about clock frequency.

I am using MCLK, SCLK, and FSYNC for I2S, and the problem is that I can't make 4MHz of MCLK.

Therefore, I can make 2 case as blelow.

Case 1

          MCLK :  3MHz

          SCLK :   1MHz

          FSYNC : 16KHz

 Case 2

          MCLK :   6MHz

          SCLK :    1MHz

          FSYNC :   16KHz

I would like to know which case can work.

Please advise me if you know it.

Thank you.