This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3204: Connection of the control IFs of the CODEC "TLV320AIC3204" and the DSP "TMS320C5504"

Part Number: TLV320AIC3204
Other Parts Discussed in Thread: TMS320C5504

I am currently trying to create a system with six TLV320AIC3204 and one TMS320C5504 connected.

In that system, I am thinking of using an SPI daisy chain for the control IF.


In TI's previous QA, the answer was that daisy-chain connection is possible, but I can't find any documentation on daisy-chain.
I can't find any documentation on daisy-chaining, so I don't know if it is really possible to connect.

Therefore.
1. is it possible to daisy-chain six AIC3204s with SPI daisy-chain connection?

2.If possible.
Is there a user guide for daisy chaining?

3.If not possible.
Is there a way to connect more than six AIC3204s to the control IF of one DSP?
Or is it not possible to connect more than six (how many AIC3204s can be connected?)?

Best regards.