Part Number: TPA3255
Hi team,
My customer needs assistance.
Dear Customer Support,
I own the TPA3255 amplifier board from Ayima (a Chinease manufacturer; the board purchased on AliExpress). Overall I quite like it. But despite this, 'just to be sure', I decided to tweak it by replacing the two input power 4700 mkF 75V electrolytic capacitors, which were installed on my board by default, with the two 70V 10000 mkF ones. But the moment I switched on the power after the replacement, the chip burned out.
The amp. board was powered with a 48V 7A Switching Power Supply unit turned up to 50 volts and had worked quite well in this mode with the board before the caps replacement.
I can add that the mentioned 48V-7A switching power supply unit remained quite alive and well in the result of the incident -- just the chip burned out.
I already bought the new TPA3255 chip for resoldering and can easily restore the original 4700 mkF caps to the board, but I would like to know the true reason behind the failure: is it something conceptual/fundamental (i.e. like 20k mkF bulk capacitance is detrimental to this design), or is it a mismath of such a huge capacitance onboard with the 48V 7A switching power, or is it just a soldering blunder that can easily be corrected, or something else?
---
Question in general: should the TPA3255 chip sustain a 20000mkF bulk capacitance when powered with 50 volts from a 48V 7A switching power supply or is it too much for it?
I'm looking forward to receiving any clue from you on this issue.
Kind regards,
Alexander,
Ukraine