Hello,
I have a customer trying to configure two PCM1865 in a master-slave 8 channel configuration running at 16 ksps.
They could get this configuration working at 48 ksps but they're running into some potential DOUT bus contention issues at 16 ksps. The DOUT pin is pulled down to about 1.8V while the rest of the signals (LRCLK and BCLK) are the expected 3.3V.
Can you recommend a slave register configuration for an 8 channel (total) configuration with a 24.576MHz clock reference on the master?
Munan