Part Number: PCM1840EVM
Other Parts Discussed in Thread: REG1117, PCM1840,
Hi Team,
Can you please help with the issue below?
A PCM1480EVM connected to DE10Standard which generates all digital clocks (BCLK, FSYNC and MCLK)
MCLK = 12MHz, see page 1
BCLK = 3.072289MHz, see page 1
FSYCK = 64*BCLK =48KHz, see page 2
The power source is a benchtop DC power supply model # CPS-3010 II feeding 5.15 VDC (see page 3) through a REG1117 regulator.
The audio captured is very noisy. The test result on page 4 shows a DFT of the PCM1480EVM i2s audio output where a tone of 4437Hz is played through a phone speaker to the onboard microphone. The pointer shows the tone of the speaker.
What is the source of the noise other than the input 4343HZ tone on page 4 of the attachment?
Please let me know if you need more information.
Thanks in advance.
Regards,
Marvin