This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3104EVM-K: Clocks modification

Part Number: TLV320AIC3104EVM-K


Dear Sir or Madam,

I'm using the TLV3320AIC3104EVM with the GUI and I'd like to modify the MCLK in order to have a Fsref of 48kHz and an fs adc/dac of 16kHz.

In order to do that, I do the following modification :

And press load. But when I measure the frequency on my oscilloscope, it is still a frequency of 11.29MHz (which is the default frequency).

How could I work on these different frequencies and see the result on the oscilloscope ?

Can I also modify BCLK and WCLK ?

Have a nice day,

William.