Part Number: TAS2764EVM
Both customer and I are experiencing low volume when testing the TAS2764EVM via the USB connection. Despite our attention to following the recommendations of the user's guide, the power we get through the 4Ω speaker is small. When using the Audacity software to test tones, I do hear good volume at a variety of frequencies.
The system is connected to 5V, with a 4-Ω speaker. The speaker signal in the scope reaches the 5V as expected. I believe the limitation in power is the result of the modulation, not a hardware issue. No modifications were made to the EVM anyway.
Is there any setting on either computer or PPC3 that we could be missing?
Thank you!