Part Number: SRC4190
Other Parts Discussed in Thread: TLV320AIC3204,
Hello the community,
i have two I2S host configured as a master (both generates LRCLK and BCLK), i want to send the audio data output of one host to the data input of the other one.
(At the origin, the interface of the host are planned to be connected to one audio codec : TLV320AIC3204)
I have no solution to synchronized the frame between each host.
Would it be possible to link the host through a SRC419x in order to sync the frame ? One host can provide a MCLK (8 * 256 kHz) as a reference clock.
The host are identical, with the same Fs : 8kHz, 16 bits per channel, BCLK = 32*Fs

Thank you for your help