Part Number: TAS2X63EVM
Other Parts Discussed in Thread: PP-SALB2-EVM, PCM9211
Hi team,
Q1. If I want to evaluate Tas2x63EVM with optical inputs, Can I use the PP-SALB2-EVM LearningBoard 2 to do so?
If yes, Would you check if below configuration is right method?
- Vbat=5V
- PVDD=11V(external PVDD used)
- 8Ohm load(dummy connected to AP)

Q2. If I connect learning board to TAS2x64EVM, Does XMOS automatically select I2S signal path from MUX?

Thanks
Jay.