Part Number: PCM5102A
Other Parts Discussed in Thread: DRV632
Hi Dear,
Our customer have encountered some problems in the process of using PCM5102A. Please help us solve them.
1. The THD+N Ratio index is required to be 0.004% (88dB), but the measured data is 0.11%, as shown in the table.

2.The frequency response from 18KHz to 20KHz drops a lot. Specific test data and pictures such as documents.
3.The following table shows the distortion indicators of PCM5102A. The maximum deviation of this chip has exceeded the requirements, but the measured results are much worse than the maximum deviation in the specification.

4. The customer has made some improvements in hardware, such as modifying the power supply; Increase the power filter capacitance; Cutting line; Reduce ESD devices; There is no obvious improvement after replacing the signal filter capacitor
5. Help to see if the audio signal amplitude used in the test is too large; Is there a problem with the setting of the test instrument?
6.The schematic diagram and layout are as follows.