This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320ADC6140: Maximum audio bandwidth (greater than 80kHz)

Part Number: TLV320ADC6140


We have designed this part into a product, built it, and only now noticed the little comment buried in the data sheet mentioning an 80kHz bandwidth limit.  Our application requires close to 100kHz audio bandwidth (2 channels). Is there a way to trick this part into exceeding the 80kHz bandwidth limit?  If not, are there any similar audio ADCs that can do 100kHz? I say "audio ADC" since we need a very low-power filtering and downsampling solution. Any ADC or ADC/FPGA combo providing this level of downsampling and filtering requires 10x the power.