Part Number: MC33078
Other Parts Discussed in Thread: LMR33630, LM5575
Greetings!
Re: MC33078 Power supply and common mode rejection ratio Asymmetry:
We have independent +15V and -15V power supplies powering several MC33078 op amps. The two supplies are generated by two TI DC converter devices (LMR33630 and LM5575) running from 24Vdc, not a multi-tapped transformer-based flyback, which would have generated synchonous supplies due to the common magnetic field in the transformer.
1) The supplies do not power up synchronously. The -15V power supply rail may take almost twice as long to power up as the +15V rail.
2) Furthermore, the -15V power supply will sometimes collapse to -11V in some cases while the +15V power supply remains at 15V.
Can we expect any damage to occur in either of the two scenarios above? Does it depend on input magnitude w.r.t. power rails?
Best Regards and many thanks in advance!
Dan Bolda
Magnetek Co.