Hi TI Teams,
Can u help to check the schematic of TPA3138D2? The schematic is as below:
And we also have one question, does the PIN2 (shutdown) can be pulled up or down all the time?
Thanks,
Kind Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI Teams,
Can u help to check the schematic of TPA3138D2? The schematic is as below:
And we also have one question, does the PIN2 (shutdown) can be pulled up or down all the time?
Thanks,
Kind Regards
Hi Lumina,
Please make sure LB800~LB804 are magnetic beads rather than 0Ω resistance. Besides this, I don't find other question.

The SD/FAULT input pin should be held high during normal operation when the amplifier is in use. Pulling SD/FAULT low causes the outputs to mute and the amplifier to enter a low-current state. Never leave SD/FAULT unconnected, because the amplifier operation would be unpredictable.
Regards,
Fengyu