Other Parts Discussed in Thread: PCM1862, PCM1861, PCM1864
Hi,
I have recently designed in the PCM1860. When I study the I2S port, I only see 16 bits of data. The rest is zero.
Is there anything I can do to get 24 bits of I2S data from it?
I have the following hardware setup:
VINL1 / pin 3 1kHz sine
All other analog inputs: floating
MCLK = 24.576MHz into SCKI / pin 15
MD0 = 1
MD1 = 1
MD2 = 0
MD3 = 0
MD4 = 0
MD5 = 0
MD6 = 0
A lot is as expected: Analog input is only applied on VIN1L and comes out on low phase of I2S LRCK. LRCK frequency is the expected 96ksps. BCK is 6.144 MHz.
Thanks,
Børge