Dears,
Customer use TPA3255 for signal channel,power is 250W with 4Ω load,Vin is DC50V,OC_ADJ is 30K, now when they do the short circuit protection then find some device is break down,pls find below information:
1. Test power amplifier has signal output, which can output 32V with 4 Ω , and then short-circuit output under full load, power amplifier chip will be burned.When they use good TPA3255 replace with bured TPA3255,function is good.
2.Set the current limit of the power supply at 0.5A, the output is not connected to the load, and then adjust the input signal to make the power amplifier output 32V, and then short-circuit output, the power amplifier chip will be burned.When they use good TPA3255 replace with bured TPA3255,function is good.
3.AP test:The low-frequency 100HZ signal input of the signal generator may burn the power amplifier chip. It worked fine after the chip was replaced.
4.After the chip OC_ADJ is changed to 64K, short circuit will not burn the chip, but it is easy to protect low frequency music playback.
5. After the chip power supply is changed to 36V, the short-circuit output will not burn, but it will not enter the protection state, and the chip will enter the thermal protection after overheating for a while.
6.Total test 280PCS,60PCS have issue.
Customer want TI help to check the schematic and PCB Layout have any issue or not.Pls kindly help.
Thanks
INPUT_SCH_1.0.SchDocPCB_AMP_V1.8_220110.PcbDocPCB_E_V1.1_201219.PcbDocPCB_INPUT_V1.1_200918.PcbDocSCH_AMP_V1.8_220110.SchDocSCH_AMP_V1.8_220110.pdfINPUT_SCH_1.0.pdf