Hi Team
for these two Pin. What is the default state during the period from power-on to the completion of functional configuration? and what is the level on default state?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team
for these two Pin. What is the default state during the period from power-on to the completion of functional configuration? and what is the level on default state?

Hello Harry,
Thank you for reaching out. After power on and before device configuration (on reset) the default for GPIO1 and GPIO2 is disabled (see Table 10-107. Page 0 / Register 98: GPIO1 Control Register and Table 10-108. Page 0 / Register 99: GPIO2 Control Register).
When plugging in the EVM to test, I observed the voltage on GPIO1 and 2 to be IOVDD. The EVM has options to install pull-up or pull-down resistors. Thus, I suspect this means that the pin is either High-Z or weakly pulled high in the disabled state.
Let me know if this answered your question.
Best,
Andrew