This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM1800: ANC system design check

Part Number: PCM1800


Hi Team,

My customer now is target to design a ANC (Active Noise Cancellation) system, and they are searching our ADC / DAC solution, need expert to provide the recommendation and technical topic reply here.

Thanks for your support in advance!

Can you help to check what are the TI hero part of ADC/DAC for below requirement ? 

-------   Requirement spec   ---------------------

  1. Group delay: <120us latency @48Khz sampling rate (ADC+DAC only, SAR ADC is recommended)
  2. ADC/DAC bit resolution: >= 14bit(applying audio scope)
  3. Port #:  ADC: 4 input (support dual channel sampling simutaneously, at least)
  4. Port #:  DAC: 2 output

<audio path> as below

BR,

Kai

  • Hi Kai,

    Questions:

    • Are they looking for CODEC or just ADC and DAC?
    • Are they implementing the ANC algorithm outside of the audio devices for example using external DSP?
    • Support dual channel simultaneously from 2 different Serial Audio Interface (SAI) or single SAI?
    • Can we request a block diagram?

    Regards,

  • Dear all:

      The reply is as following

    • Are they looking for CODEC or just ADC and DAC?
      • >> We also look for CODEC but group delay(<120us@48k) all cannot meet our requirement.  Is there any suggestion? 
    • Are they implementing the ANC algorithm outside of the audio devices for example using external DSP?
      • >>Yes, using external DSP
    • Support dual channel simultaneously from 2 different Serial Audio Interface (SAI) or single SAI?
      • >> If use single SAI.  Will it impact sampling time simultaneously.  or It's only transmission time impact?
    • Can we request a block diagram?
      • >> block diagram will be like audio path illustration. 

    Thanks!

    BR/Elvin

  • Hi,

    The current codec has group delay greater than 120us. I'm checking internally if we have ADC/DAC that will meet your requirement.

    Single SAI will have the same sampling for both channel.

    Regards.

  • What is the end application that needs such low latency? 

  • Hi PD,

    This is a education cooperation case, the education side requires such a specification.

    I guess that is for the ANC purpose ? In order to implement the noise cancelation, it need the real time sampling signal ? Is this make sense?

    Or if for ANC system, what kind of the latency here in your experience before ?

    Thanks!

    Kai

  • Our device currently running like 350us or more, I have never seen such low group delay requirement for ANC.

    We might not be able to support that with current device.

    We have newer devices coming later this year below 120us, what is their timeline and the company and application details in a private message?

    Regards.