This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS2X63EVM: Warning message display in application

Part Number: TAS2X63EVM

Hello,

We connect TAS2X63EVM Kit with PPC3 Application. When we open application then it gives message that you have different versions of EVM.

  

  • Hi Deepa, 

    this error can  be ignored. it will not affect the GUI function or device performance.

    the reason for this error is because the Hardware ID this is programmed into the EEPROM on the EVM and the HWID that the PPC3 GUI is looking for do not match. 

    We are working to fix this for all future EVMs. 

    Regards,
    Arthur