Part Number: PCM9211
Currently, I'm using Bin Tool to set registers for the PCM9211. But, I'm not clear how to use it to set audio path from AVIN / SPD/IF / MPIO-B to MAIN OUT, how to config registers for PRE_POWER_UP, and PRE_SHUTDOWN.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PCM9211
Currently, I'm using Bin Tool to set registers for the PCM9211. But, I'm not clear how to use it to set audio path from AVIN / SPD/IF / MPIO-B to MAIN OUT, how to config registers for PRE_POWER_UP, and PRE_SHUTDOWN.
Hi Jeff
I think this thread want to support how to set the registers on AVIN / SPD/IF / MPIO-B to MAIN OUT.
Several weeks ago, I have already released the code to Zimin. Now, his code has been already integrated into his platform.
He began to set the register to debug the pcm9211.
BR
Shenghao Ding
Hi Zamin,
Usually the best way is to use the dedicated GUI as you can change the configuration and get the registers set up without doing much work.
If you want to write the script and feed it to the a general I2C master , attached is the general (initial set up that can be used .You can modify it according to your needs .

#************************************** #this script is for SPDIF-->RXIN0-->DIR-->MainOutput, Record sound from SPDIF to PC through TAS1020 #So #1, Chose RXIN0 to DIR #2, Active DIR #3, chose DIR output as Mainoutput's source. #Also HW modification #1, Flying to High Level(3.3V) to make sure U7's output is Hi-Z #or 2, TAS1020 output logic high on P1.2 I2S enable signal. #************************************** #System RST Control #w 80 40 00 w 80 40 33 w 80 40 C0 #XTI Source, Clock (SCK/BCK/LRCK) Frequency Setting # XTI CLK source 12.288 and BCK 3.072, LRCK 48k = XTI/512 w 80 31 1A w 80 33 22 w 80 20 00 w 80 24 00 #ADC clock source is chosen by REG42 w 80 26 81 #XTI Source, Secondary Bit/LR Clock (SBCK/SLRCK) Frequency Setting w 80 33 22 #********************************************************* #-------------------------------Start DIR settings--------------------------------------- #REG. 21h, DIR Receivable Incoming Biphase's Sampling Frequency Range Setting w 80 21 00 #REG. 22h, DIR CLKSTP and VOUT delay w 80 22 01 #REG. 23h, DIR OCS start up wait time and Process for Parity Error Detection and ERROR Release Wait Time Setting w 80 23 04 # REG 27h DIR Acceptable fs Range Setting & Mask w 80 27 00 # REG 2Fh, DIR Output Data Format, 24bit I2S mode w 80 2F 04 # REG. 30h, DIR Recovered System Clock (SCK) Ratio Setting w 80 30 02 #REG. 32h, DIR Source, Secondary Bit/LR Clock (SBCK/SLRCK) Frequency Setting w 80 32 22 #REG 34h DIR Input Biphase Signal Source Select and RXIN01 Coaxial Amplifier #--PWR down amplifier, Select RXIN2 #w 80 34 C2 #--PWR up amplifier, select RXIN0 w 80 34 00 #--PWR up amplifier, select RXIN1 #w 80 34 01 #REG. 37h, Port Sampling Frequency Calculator Measurement Target Setting, Cal and DIR Fs w 80 37 00 #REG 38h rd DIR Fs r 80 38 01 #*********************************************************** #------------------------------------ End DIR settings------------------------------------------ #*********************************************************** #---------------------------------Start MainOutput Settings-------------------------------------- #MainOutput #REG. 6Ah, Main Output & AUXOUT Port Control w 80 6A 00 #REG. 6Bh, Main Output Port (SCKO/BCK/LRCK/DOUT) Source Setting w 80 6B 11 #REG. 6Dh, MPIO_B & Main Output Port Hi-Z Control w 80 6D 00 #*********************************************************** #------------------------------------ End MainOutput settings------------------------------------------ # read back all registers to ensure GUI integrity r 80 20 5E
Regards,
Arash