Hello,
Does TI have any good IC:s (or combos/solutions) that can do the following?
1. Input 6 channels of S/PDIF and 1 channel of I2S.
2. Multiplex and up-sample these and decide which one to transmit via I2S.
3. Support sample rates up to 192 kHz and 24-bit data.
4. Support reading the input sample rate of each channel individually, without having to activate/transmit that channel.
Help appreciated!
Regards
Jack