Part Number: TLV320DAC3120
When creating a short circuit at either output of the TLV320DAC3120, the device suspends operation as it should, but both customer and I don't see the register P1R32 being updated. I'd expect bit 0 to flip to a "1" when the output is shorted, but it doesn't. This happens with the EVM and with a custom board. Is there a specific procedure we might be missing to read P1R32 bit 0?
Thank you!