Part Number: PCM1753
Other Parts Discussed in Thread: PCM1780, TLV320DAC3100
Hi, TI support team
I am looking for a solution including an Audio DAC to output an alarm sound to an e-cigarette.
The basic concept is to send the sound source to the DAC through I2S and output the audio by attaching a speaker to the DAC output.
It seems that the PCM1753 and PCM1780 products have analog output pins and can output 4Vp-p and 3.9Vp-p respectively.
Is it possible to compose like the simple block below?
The speaker is intended to be configured with a specification of about 0.5W.
Do I need Audio AMP between DAC and Speaker?
If there is a better, simpler way, please advise.
Also, if there are other suitable parts other than the parts mentioned above, please recommend them.
Thanks.
Regards,
MJ