This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3255: TPA3255 Mono Output watts @ 8 Ohms?

Part Number: TPA3255

I'm working on building a Class-D Bass guitar Amplifier. I need to know what is the real world mono-output of the TPA3255 @ 8 Ohms. 

  • Hello Ervin,

    What supply voltage are you looking at. Given you using a high impedance, for mono or stereo the max 8 ohm output power would be about the same because you would be voltage clipping around the same point. The additional output current capabilities from PBTL wouldn't really come into play.

    Also I don't know you mean by real world mono output, all of our datasheet performance measurements are validated on the actual device.

    best regards,
    Luis

  • I guess my question is what wattage can I publish to spec giving the maximum 53 voltage for a amp to run a 8 ohms mono? 200w , 300w??

  • Hi Ervin

        For 8ohm load, the current ability is not the limitation, no matter you use BTL or PBTL, 150W is the Max power you could get without clipping. Because the amplifier output voltage can't higher than PVDD voltage, if you want higher power on 8ohm load, you need much higher supply voltage, which is out of spec of this device.