Part Number: PCM1864-Q1
Hi team,
Would you please check the In/Out configuration of PCM1864-Q1?
A customer wants to use DOUT for input#2, input#3 and DOUT2 (GPIO3) for input#1 from MIC using I2S mode.
In that case, the following configuration is correct? And are there any other register settings for DOUT2?
DOUT :
Page 0: address = 0x06 (SEL_L) -> 00 0100: VINL3[SE]
Page 0: address = 0x07 (SEL_R) -> 00 0100: VINR3[SE]
DOUT2 :
Page 0: address = 0x08 (SEL_L) -> 00 0000: No select
Page 0: address = 0x09 (SEL_R) -> 00 0001: VINR1[SE]
Page 0: address = 0x11 (GPIO3_FUNC) -> 101: DOUT2 (Out)
Page 0: address = 0x13 (GPIO3_DIR) -> 100: Output
Thanks,
Sam Lee