This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCM9211: Timing chart

Part Number: PCM9211


Hi,

Customer inputs the I2S signal from an external device into the PCM 9211.
And the customer wants to input the I2S into the DIT and do the SPDIF conversion.
Could you answer the following questions?

1. Could you tell me the timing chart of BCK/LRCK/DATA in DIT when I2S is entered?
2. Also, is my understanding correct that I refer to page 10, 6.8 Timing Requirements for the value (min/max)?

Best Regards,

Nishie