Part Number: PCM5101A
Other Parts Discussed in Thread: NE5532A
Hey Team,
Have a few questions for you
- It states that the minimum load is 1K. and typical output voltage is 2.1V. So, it can drive only 2.1mA in 1K load or generate 4.41mW audio power at 1K. Am I understanding that correctly?
- Since my application requires 80 mW at 600 ohm, does it mean I need an audio amp? Any suggestion?
- Looks like the development board has the same schematic as in Fig 33 of DS. What is the purpose of 470 ohm in parallel with 2.2nF or 2200pF is limit the BW to about 1MHz?
- Why is there 100K pulldowns on I2S bus in development board?
- If we tie OUTL and OUTR nets past the 470 ohm resistors together, will that double output load current to 4.2 mA?
Thanks!
Cameron