Part Number: PCM2900C
Hi,
I am designing a USB to Stereo audio module and would like to use one of the ICs in the PCM290xC family.
The design shall be industrial temp (-40*C to 85*C).
Is there any known problems when going below -25*C?
Is it ok to cold start the device at -40*C and use the device as normal when the temperature reaches -25*C?
Can you provide any test results from -25*C to -40*C or any information about performance?
Thank you!