Page 0 / Register 4 / bit D6 allows you to set the PLL range
0: Low PLL Clock Range
1: High PLL Clock Range
When should this bit be set to 1 instead of 0?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Page 0 / Register 4 / bit D6 allows you to set the PLL range
0: Low PLL Clock Range
1: High PLL Clock Range
When should this bit be set to 1 instead of 0?
Hello Douglas,
The TLV320AIC3206 offers a wide range of clock frequencies. Setting this bit allows the user to extend the high "1" or low "0" bounds at the edges of the PLL clock range.
As described in 2.7.1 PLL:

I hope this helps.
Best,
Andrew