This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All
As part of the project, I need to decide whether I will separate ground planes under PCM2904 or not.
The Power 5V planes were separated accordingly.
Please see the image: separated groundes with a simple ferrite bead that can be assembled as 0R.
Is there truth in things or to tie the ground planes together without being clever? Please review
BR
Baruch