Part Number: LM4861
I am having problems with crossover distortion with this amplifier. We have it set up like it is in the typical application figure 2. However, for Rf we are using 100k and for Ri we are using 40k. We are getting this weird blip at the crossover. I hooked up a potentiometer to the line to see how the resistive load affects its. It looks like the glitch starts happening at about 107 ohms. Anything over 107 ohms I get a clear waveform. Whenever the potentiometer was below 107 ohms the cross over distortion would start and continue to get worse as resistance decreased.
Does anyone have any experience dealing with crossover distortion in these amplifiers?
CH1 is differential between pins 5 and 8
CH2 and CH3 are the signals at pin 5 and 8 respectively.

Thanks,