This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC3268: Questions of TLV320AIC3268

Part Number: TLV320AIC3268

Dear team,

Do we have suitable solution can meet below spec?

This case only needs the input/output two-channel audio codec for the amplifier application, and the design will need to use 2 sets of I2S, if the price is competitive, please recommend suitable materials, thanks

- Type: audio codec ADC/DAC
- Bit resolution: >= 24 bit
- Conversion Rate(fs): >= 96 kHz
- ADC analog inputs: 2 channels (support single-ended)
- DAC analog output: 2 channels (support single-ended)
- ADC input voltage: > 1 vrms, > 2 vrms is better (single-ended)
- DAC output voltage: > 1 vrms, > 2 vrms is better (single-ended)
- ADC SNR: >100dB
- DAC SNR: >100dB
- ADC THD+N: < -90dB
- DAC THD+N: < −90 dB


Or hope to recommend independent ADC and DAC solution, thanks

Jimmy