This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5754M: Amplifier output

Part Number: TAS5754M
Other Parts Discussed in Thread: TAS5828M

Hi,

I'm trying to set up a TAS5754M in my own PCB.

I have PPCMB with TAS5754M Evaluation Module. My LRCLK = 176.4kHz, BCLK = 11.2896MHz, Fs=176.4kHz

Mono Amplifier Application Schematic and PurePath Console2 is  being used.

To enable 3-wires I2S I use:

w 9a 00 00

w 9a 02 10

w 9a 25 18

w 9a 0D 10

w 9a 02 00

The amplifier works. The sound is heard.

 Then I dump registers to the config file and write it to the own  TAS5754 via I2C.

The amp tries to play but shuts down and tries to play again. Repetition cycle about 1.5s. See the picture (only one cycle is shown).

 I checked the voltages on my board and TAS5754M Evaluation Module They are the same.

I read and compare values ​​of the registers (only  Page 0) on my board and  Evaluation Module  they are also the same.  Measured CPf=1.4112MHz  (Identical on TAS5828M Evaluation Module  and  my board).  

 Maybe you can advise what I am doing wrong.

 Thank You

 Gailius